• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Power Management » AC/DC and Isolated DC/DC Power » AC/DC and Isolated DC/DC Power Forum » UCC28070 problem
Share
AC/DC and Isolated DC/DC Power
  • Forum
Options
  • Subscribe via RSS

UCC28070 problem

UCC28070 problem

This question is answered
Marius Apetrei
Posted by Marius Apetrei
on Jul 24 2012 14:32 PM
Prodigy30 points

Hi all. We are testing a new design based on the ucc28070 controller, which is very similar to the PR779 1,2 kw PFC and having difficulties. On the first two tests the mosfets on one phase have blown up (very high input currents, large output voltage fluctuations with peaks of over 1000v and also sounds coming from the inductor). Each time the ucc28070 was also affected, as between pins 15 and 17 we measured a small resistance (22ohms aproximately). We were using MCP1407 to drive the mosfets, but now we switched to a 2-transistor buffer because the drivers also blew up.

On the third test we disconnected both mosfets and supplied power only to the ucc. we also supplied Vsense with 1,3V to keep the circuit running.

Without applying any voltage on the CSA and CSB pins, the duty factor was the programmed maximum (90%). When we applied voltage to CSA (0-3V) , the duty factor started to decrease with increased voltage.The decrease started at about 1,4V.

The VINAC pin seemed very sensitive as even a very small voltage (milivolts) caused the duty factor to go maximum and stay there regardless of the voltage being disconnected afterwards. We mounted 4,7nF capacitors on the VSENSE and VINAC pins. The threshold at which the duty factor started to decrease was not 1,4V anymore but 0,8V.

We observed that if we apply voltage to both CSA and CSB the threshold moved back to 1,4V.

The circuit seemed insensitive to VSENSE voltage variations up to 3V , value at which it went into OVP. 

  Another yet more important problem is that any AC voltage applied at VINAC caused the duty factor to go to maximum (shouldn't it vary with applied voltage, going up close to the zero crossings and down on the peaks?).

The values were calculated using ucc28070 excel design spreadsheet. We took a close look at the pcbs and there is no error there. The ucc was soldered with hot air in the minimum amount of time. We have experience with switchmode power supplies and designed the circuit with regard to the PR779 evaluation board layout. The inductors used were wound on 2 T200-2 cores each with a inductance of 130uH. Current transformers were wound on 43 mix ferrite cores at a 1:100 ratio.

Thanks in advance for any suggestions.

Regards

Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • CWilson
    Posted by CWilson
    on Jul 25 2012 02:40 AM
    Expert1730 points

    When Vsense is 3V, the UCC28070 is in regulation - e.g. at 400V output.

    Do you have leading edge blanking on your current sensors or some sort of damping of the ringing from the inductors?

    Could you provide a schematic?

    Use only 1nF on VINAC. Don't apply caps on your Vsense. If you use caps, the regulation will be slower.

    Try to use the SI8503 instead of the current transformers. And then adjust the signal level on PKLMT (peak limit). The SI8503 gives 2V output at max current - e.g. 20A measureing = 2V out. This signal you can compare to PKLMT (use resistordivider from VREF (6V) to PKLMT) to match max current through MOSFETs/SI8503.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Marius Apetrei
    Posted by Marius Apetrei
    on Jul 25 2012 12:50 PM
    Prodigy30 points

    Hi, this is the schematic we are using right now.

    Regarding your suggestion to use SI8503 we currently do not have this component and would like to stick with the current transformers for simplicity.

    We do not have leading edge blanking on current inputs as you can see; the damping networks would have been added during testing ... if only it would work without blowing up ... 

    I forgot to mention on the second test we used only 50Vac at input with a small load of only 5kohms. The idea was to ramp up slowly the input voltage after we measured some waveforms on the circuit and made sure everything is ok but no luck.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Adrian Stevens70553
    Posted by Adrian Stevens70553
    on Feb 15 2013 11:08 AM
    Prodigy40 points

    Hello Marius,


    Did you get this problem resolved?  We are looking to use this part too and wondered what the problems are?

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Marius Apetrei
    Posted by Marius Apetrei
    on Feb 16 2013 13:38 PM
    Verified Answer
    Verified by John Bottrill
    Prodigy30 points

    Hello Adrian,

    Sadly no ... after having spent many long nights, we could not get it to work properly and due to time constraints we abandoned this project to focus on more lucrative ones. As far as we got, it's not blowing up any more expensive mosfets but the input current distortion is horrible and we didn't bother to test at higher power levels. Overall the circuit as a whole is extremely sensitive, not something I would put in production. That is just my opinion and limited experience, maybe others with more knowledge could be able to make it work ok.

    All the best

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use