5611.LM5022 Wide Input design .pdf
HI,
Kindly verify the transformer design for this wide input power supply using LM5022
Regards
Atul Bhakay
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
5611.LM5022 Wide Input design .pdf
HI,
Kindly verify the transformer design for this wide input power supply using LM5022
Regards
Atul Bhakay
Hi, Thanks for your suggestion. But, with a turns ratio of 12 and the peak secondary current being 4.8 AMps, the peak primary current will be 4.8 / 12 = 0.4 Amps , which is TOO................... LESS.
I have assembled the board with the transformer as per my calculations. The power supply is starting up at 35V ac or 45VDC, but not at the designed 17VDC. What could be the issue ? KIndky advise
Regards Atul Bhakay
Hi,
The power supply is ‘starting’ at 35VAC or 45VDC but not at the designed 17VDC. (this start up is on no-load)
Subsequently, the PSU operates up to the high line i.e. 265VAC
With ref to the schematic (attached herewith) do the R2, R7 , R39 resistors need to be altered ? Or does the transformer need to be changed ?
2364.PSU BOARD V3 0 SCH (3).pdf
Regards Atul Bhakay
The resistors in the voltage divider are too big in value, and Q8 does not have enough base current... Delete Q8 and R42, tie the UVLO pin directly to the 5.6 Zener, and change R39 to 12.4k, and reduce R2 and R7 by 10x. Do not forget to use higher power rating resistors for R2 and R7.
Thanks,
Youhao Xi, System and Applications Engineering, TI SVA-PPD
Hi, there is no improvement in the start up of the power supply even after incorporating the suggestions. I have now modified the primary inductance from 283uH to 160uH. I am still awaiting the transformer details of PMP7760
Regards
Atul bhakay
For LM5022 to start, you must have the VIN voltage at least at 6V. D6's leakage current may cause too much voltage drop across R3 and R8, and D6 and Q7 cannot not produce 6V for VIN when the input is at 12V input. Please check VIN pin voltage.
Thanks,
Youhao Xi, System and Applications Engineering, TI SVA-PPD
Hi There;
I am looking to use the Isolated LM5022 device to be used an Wide Band Input up to 800V - the same as the PMP7763 which is on the TI website.
The only difference I am looking to implement is the Output Voltage - Rather than having 24V 250mA - I am looking possibly of steping down further to 5V@ 200mA
Can this be done??
Paul.