hello I´m using a MC34063 to elevate 24v to 32v DC and my maximum output current is 80 mA, But when I put a load that consumes 11 mA, the MC34063 got very hot, is this behavior normal?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello I´m using a MC34063 to elevate 24v to 32v DC and my maximum output current is 80 mA, But when I put a load that consumes 11 mA, the MC34063 got very hot, is this behavior normal?
Jose,
That is not normal. Check pin 1 to see switching quality.
Did you use a Rsc? Is the diode a Schottky?
Please list the support components used.
If possible, pin 1 waveform would be helpful.
yes I'm using Rsc = 1 ohm, and my diode is the same that the datasheet proposed (1n5819).these are my design parameters
Vin = | 24.00 ±26% V |
Vout = | 32.00 V |
Iout = | 0.08 A |
Vripple = | 0.10 V |
I attach the components that I have calculated and the components that I've used:
L=680uH
Rsc= 1 ohm
Ct = 470pf
R1= 1.2 k
R2= 30k
C0 = 100 uF
and I don't have a image from the waveform of the pin 1, the resistence that is conected in the pin 8 got hot, the input current when I put the load was 42 mA and the output current was 11mA. Thanks for answer
Jose,
I believe the base of Q1 is being overdriven creating long turn off time (see notes on page 4 of data sheet).
I suggest changing pin 8 resistor to 18V/22mA = 820 ohm. This gives 22mA to Q1 and Q1 base resistor with minimum VIN. 22mA=7mA+(0.3V/1ohm)/20.
I have come across the problem posted by Jose Morales (Sep 06 2013) and an answer posted by gone Ron Michallick (Sep 09 2013). It is about a year now since their communication and hopefully Jose might have solved the problem. However, I wish to add that the circuit should function better by connecting Q1 and Q2 in Darlington form as suggested in the literature. This will reduce the turn off time of Q1 that has to switch the maximum portion of peak current.
Also 1N5819 should be replaced by schottky diode rated for 1 Amp, PIV 100 Volts. Look for diodes from MBR series or SR series.