Hi TI,
I am in the beginning of designing a 1u height PSU that can deliver up 1200W output power. It is almost similar to the PSU datasheet attached.
With this low profile, a high efficiency at least 95% for DC/DC and 95% for PFC is needed so that the heatsink size is small enough. Combining these 2 efficiency, the total efficiency of whole PSU should be more than 90% at rated load.
Do you have any design idea (what topologies, which TI IC) for the PFC and for the DC/DC that is in small form factor and can deliver 95% efficiency?
Regards,
KK