I am design a DC/DC power module use LM5118 ,VIN 9-48V ,Vout 53V/0.5A ,NOW when i slowly increasing the load(<0.5A), there is no vout suddenly,and LM5118 is damaged, always feet 16 and 18 feet breakdown,then i try to put a schottky diode between 16 and 18 feet and increase the load,feet 10 breakdown,pls help check my SCH and give me a hand。thanks!1222.LM5118设计原理图.pdf