Customer found the some issues on UCC28630EVM.
1. We found voltage Regulation Problem at No load as below, how to improve it? Is it caused by the PSR topology?
At 115VAC: 19.7~19.78V, 19.82~19.85V; At 230VAC: 19.74~19.78V, 19.88~19.91V
2. After R18 is removed, the output voltage cannot be well regulated and the OVP would be triggered. Why?
3. During power On/OFF test, the power supply will be shutdown. How to improve this?
4. Voltage Regulation is not good during 0% to 100% transient load. Even not good during 50%~75%. Is it because PSR topology leading to pool regulation? Please see the waveform as attached.
5. Why the Electronic load needs to be set with constant resistance mode? Below definition is from EVM user guide. Can it set with Constant voltage Mode Electronic Load?
Regards,Brian