Is there an automotive qualified version of product - TPS55010, 2.95V To 6V Input, 2W, Isolated DC/DC Converter with Integrated FETS, available or in development ?
- Tapajit
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Tapajit,
The team that owns this device will have to answer. I'm going to move the question to their forum. I know the SN6501 isolated power supply has an automotive version SN6501-Q1.
- Scott
Hi Tapajit,
There are no plans I know of to qualify the TPS55010 or similar part as -Q1. Do you have some details you can share on the application?
The SN6501-Q1 Scott mentioned can typically work in the same applications. Can you use this instead?
Thanks,
Anthony