The two phases (lets call them A and B) of a buck converter will not work together. Each phase will work fine when the other is disabled. When both phases are enabled only phase A works--Phase B will not start switching. If I turn disable Phase A by remvoing the MOSFET, Phase B will work with no problems.
The design uses two UCC27201D MOSFET drivers in the conventional buck topology (i.e 1 MOSFET, 1 diode). Both UCC27201D are power by 12V and both use a 0.1uF boost capacitor. The input voltage is 56V and the output voltage is about 24V. The design switches at 250kHz.
Any Ideas?