I'm designing a Isolated Flyback DC-DC converter.
Vin: 32V to 60V, typical voltage: 48V
Vo: 24V
Output Current: 1.4A
I have selected LM5021 as of now.
I need help with the design. Is LM5021 correct choice? or any other better part?
Jai.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm designing a Isolated Flyback DC-DC converter.
Vin: 32V to 60V, typical voltage: 48V
Vo: 24V
Output Current: 1.4A
I have selected LM5021 as of now.
I need help with the design. Is LM5021 correct choice? or any other better part?
Jai.
Hi Jai
There is a TI reference design available, http://www.ti.com/tool/pmp7917.1#1 this is a 25W design with dual output so the transformer will have to be redesigned for the higher output voltage and power but it should give a good starting point.
Regards
Peter