Hi,
Here I got a question about the overcurrent threshold of UCC2808 from customer. Here is his testing result:
@ Room Temperature:
No. |
0009 |
0011 |
0012 |
0013 |
0015 |
Overload current |
1250mA |
1290mA |
1230mA |
1200mA |
1300mA |
@ 65 degree:
No. |
0009 |
0011 |
0012 |
0013 |
0015 |
Overload current |
1180mA |
1220mA |
1170mA |
1150mA |
1240mA |
@ -15 degree:
No. |
0009 |
0011 |
0012 |
0013 |
0015 |
Overload current |
1260mA |
1290mA |
1230mA |
1190mA |
1290mA |
My questions are:
(1) Is the above testing result meet with the tolerance of CS threshold?
(2) What is the CS threshold tolerance of UCC2808?
(3) How much will the temperature influence this tolerance?
Waiting for the response... Thanks very much!