Does anyone know a regular Voltage Mode Control Chip for buck converters? Single channel PWM output is enough. It is not common nowadays.
Sam Guo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sam,
You can use the 3843 type parts and run them in voltage mode by driving the CS pin using the slope compensation circuit setup such that the input to the CS pin ramps from 0V to 1V.
Regards
Peter
Sam,
I've used the UCC25701 in a AC DC forward. It can be used in a buck converter topology. The chip has a built in feed forward circuit and volt -sec clamp. The built in feedforward provides excellent line rejection -just as good as current mode control. You have to supply your own error amp as the input goes straight to an uncommitted comparator. I like this about the UCC25701. If you have a cost sensitive design you can use a sot23 tlv431 for the error amp. If you need high performance you can choose a high speed op amp.
Good luck with your design,
Chuck
What is the part number? UC3843 is a Current Mode Controller, not Voltage Mode.
Sam
Dear Chuck:
That is a great controller. I like it very much.
I appreciate your help.
Sam