Hi all,
I am trying to test the current loop of uc3886 and left voltage loop open. Based on the application note u-156, the voltage error amplifier output range is from buffer voltage-0.7 to buffer voltage+1, however, I tried to connect both command pin and buffer pin to the ground and set sense pin high, the comp pin is about 1V. After this, I also tried to connect 0.35V via VREF to the comp, the voltage on the comp pin is still around 1V. For my current loop test, the comp should be 0.35 to verify the current loop.
My question is that is it possible to get comp voltage lower than 1V? Also, from the electrical charateristic chart, the output range is from 1.9 to 4.1, which conflicts with my measurement.
He, Siyu