I have a quesion of ZCD current limit value, 10mA or 1mA.
In datasheet page 8, "Zero Current Detecion and Re-start Timer Blocks" column, 4th line sentese said;
"The resistor value in series with the secondary winding should be chosen to limit theZCD current to less than 10mA."
Meanwhile, datasheet page 16th, "Zero Current Detection" clumun, second line said;
"This pin (means ZCD pin) has clamp at approximatery 5V. Add a current limit resistor, RZC, to keep the maximum current below 1mA."
Which of 10mA or 1mA is correct?
Pls advice.
Thanks
Rick Zaitsu