Please let me know about Icc max of LM5020.
For example, Icc (at Vin:48V) is written on the datasheet figure-4.
But I want to know Icc at Vin:15V condition.
【Supplement】
・Vcc connects to a photocoupler.
・Photocoupler's Maximum rating:20mA, Operating range:5~10 mA.
・A customer's ideal Icc is more than 20mA.
Best regards,
Satoshi