TI's reference design TIDA-00173 uses UCC28711 with input voltages of upto 1.2kV DC. Since the HV start-up pin can withstand upto 700V input only, a resistor network along with a TVS diode has been used on the HV pin. I am designing a power supply for a similar input voltage range and wish to use UCC28710. My question is, do we need an additional zener diode to clamp the input voltage at the HV pin? If not, then how is the voltage being regulated at the HV pin? As far as I know, we cannot use TVS diode in continuous breakdown region.