I have two buck converters, with Vin = 28V and Fsw ~ = 150 kHz, that are connected together for a +/-15V power supply. The RMS current in the output capacitors (3 X 22 uF tantalums in parallel on each rail) is calculated to be 152 mA, so ~ 50 mA RMS per capacitor.
The failure rate of the capacitors has been higher than expected, possibly due to 25V rating on the caps (slightly underrated voltage for 15V output) and possible cap manufacturing issues. They are being replaced with 35V caps (15 uF) and the results so far are promising.
However, there have been a few cases where all 3 caps on a rail were blown, even with the new and improved caps. Also, I've looked at the failure statistics and there are ~50% higher failures from one set of loads as compared to another set of loads. I haven't done the research to determine the differences in load types and magnitudes. The temperature environment is more benign for the case where more failures occur.
Two questions:
1. What event(s) would blow 3 parallel caps on an output?
2. Could RMS cap current be remarkably higher with some load types compared to others? What load types?
Thanks,
Jeffrey Bledsoe