Is there a way to keep a fixed switching frequency on UCC28610 regardless of the load?
Or at least keep it above 60KHz. The switching freq on AM mode is causing noise on my device.
Any help is appreciatted.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there a way to keep a fixed switching frequency on UCC28610 regardless of the load?
Or at least keep it above 60KHz. The switching freq on AM mode is causing noise on my device.
Any help is appreciatted.
Hi Peter,
The application is not audio. I'm powering a sensor that is affected by switching frequencies below 60KHz.
I'm trying to stay away from those frequencies without having to change the controller.
The UCC28610 can be configured for constant switching frequency by connecting a resistor from FB to VDD for a fixed FB current. Control has to be done by using the MOT pin. The MOT has to be used to modulate the on-time by connecting it to the opto-coupler, instead of connecting the FB pin to the opto. A resistor is connected to MOT to ground for the maximum on time, then the collector of the opto is connected to MOT with a series resistor for constant on-time control, essentially varying the MOT total resistance.