Hi,
I need to simulate my schematic in TI TINA tool. I have downloaded version 9.
Input: 20VDC to 75VDC
Output: 12V/3.4A
Transformer: EFD25
Topology: Forward converter
Switching frequency: 250KHz
Device: UCC2897A
I need to model the forward converter transformer, please suggest me which option I need to select in the Transformer option in schematic editor tool like ideal transformer, non linear transformer.
I have attached here the schematic file. while running ERC is zero but while doing DC analysis (table of DC results) simulation, it will get stuck in the middle and giving an error.
Please suggest me on forward converter transformer modeling and circuit simulation.
Regards
KiranKumar BG