Hello, I'm planning to synchrozine multiple TPS55010 on a single board. And want to use this approach:
The U2 is a buffer with 3-state output control.
I will activate buffer output only for synchronization. Is it normal to have direct dc-coupled connection of driver output with RT/CLK input (the situation when buffer output is active but RT/CLK internal 0.5V voltage source hasn't been removed yet)?
Thanks.