Dear All,
I am using UCC28711 IC for my flyback SMPS design having primary voltage range 400-800V DC and output voltage 110V,1.25A ( single secondary).
I am following tidu412a.pdf file as my reference design.
while giving the DC bus voltage near about 430V, I am observing the VDD of the UCC28711 swings between 21V to 14V. And also HV_start pin swings between 370V to 25V. It seems to me that PWM controller IC UCC28711 is not enabling up properly. Also the IC is also releasing only one Gate pulse, however in the UCC28711 datasheet and also in TI design document the IC releases three pulse at start up. The IC is entering in START up mode again & again and hence the VDD varies between 21V to 14V.
Can it be a problem of IC or xmer design.
Please help
Regards