Hello
Socomec, one of my customer is working on Electrricity Circuit breaker and will use a motor to control this equipment.
Input voltage is single phase 300 to 570Vac (400 to 820V DC) to generate a 24V isolated 400 to 600W.
They are looking the UCC25600.
They have already posted a E2E ads "Question on UCC25600 and SLOU293C: 600W isolated PFC power supply..."
Is the UCC25600 the best part to suggest?
One of the point of interest for Socomec is they do NOT prefer to use frequency above 150kHz but need to have for so low frequency Burst mode.
It seems that if they limit the switching frequency at as exemple 100kHz but external resistor RT modulation, in such case if Vin increases then we can have no output regulation. Solution can be to have Burst mode but normally not at such low frequency.
Question is How to have working conditions including Burst mode with frequency lower than 150kHz?
Thanks to let me know or suggest another solution.
Thanks for your help and best regards
Jean-Paul