in order to see ucc28700 functioning ,i have connected cs pin and cbc pin to the ground and applied 21 v to Vdd pin.
i am able to recieve only one pulse.but accordind to datasheet i should get three pulses.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
in order to see ucc28700 functioning ,i have connected cs pin and cbc pin to the ground and applied 21 v to Vdd pin.
i am able to recieve only one pulse.but accordind to datasheet i should get three pulses.
The IC looks for a change in slope on the Vs pin voltage to terminate the off time. This change in slope is called the Demagnetisation ring becuase it happens when the flux in the core has been depleted and the core is demagnetised. If there is nothing connected to the Vs pin and the IC does not see this ring, then it will not switch.