Hi All,
Can someone explain what is the difference between the dead-time generated with LM5106 and LM5106?
Thank you
Leo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Leo,
The most important differences are: LM5104 integrated the boot strap diode; Enable function; Deadtime control;
Other differences include ESD ratings, peak pull up current , .etc can be found by comparing the electrical tables.
Br
Hi Leonardo,
tHPLH is the Upper output(HO) turn on propagation delay, and tLPLH is the Lower output(LO) turn on propagation delay, both of them are refer to the Input and including the deadtime set by the RT resistor, so there are the total delay times as you understand. Thanks!
Best Regard,
Oliver