I want to design a solar power bank for my final year project any one help me to suggest safety feature required and efficient design for circui
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to design a solar power bank for my final year project any one help me to suggest safety feature required and efficient design for circui
Thank you for your reply but that product is support for solar panel which have capacity of 28V and above and here in my project we need only 5 V solar panel so it will be difficult to use this product.
Would it not be a simple task to stack the outputs of 6 solar panels to get 30V? Or could you not use a 5V to 28 V DC DC converter? This is often done in the industry. In fact this is how I designed the Solar Panel Grid Tie PS for Petra Solar. You can use a synchronous buck/boost converter with greater than 95% efficiency to convert the 5V output to 28V. Or you can stack the solar panel outputs.
Chuck
No i Only want maximum 5V output from My solar panel to charge Li-Ion Battery. and that stored power will charge my smartphone or ipad using usb cable that is my basic concept.
Input from solar panel Max 5V-Store in Battery- output to smartphone or tablet
So main three circuit will be use
1) CHARGING CIRCUIT BUCK CONVERTER
2) BATTERY PROTECTION CIRCUIT
3) BOOST CONVERTER