This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3854 not giving pulses

Other Parts Discussed in Thread: UC3854, UC3854A, UC3854B

Hello everyone, I am here to ask some questions about a boost PFC circuit with UC3854 as a controller. I attached my schematic design.

This is for 2000W power output. My AC line is 170- 270V and 45-55Hz. My Inductor is 1mH and output cap is 2x470uF.

Shunt resistor (Rs) is 50 mR, Peak curent limit is 20A and switching frequency is 52kHz. 

Below is the other important values that I used.

Name Ref. Value
Rvi R75 470K
R81 56K
Rvd R87 10K
Rs R64 100mR
R66 100mR
R70 -
Rvac R89 620K
Rb1 R86 150K
Rvf R94 27K
Rff1 R88 1M+27K
Rff2 R93 180K//56K
Rff3 R91 10K
Rset R95 4.7K
Rmo R85 1.2K
Rci R103 1.2K
Rcz R100 33k//33K
Rpk2 R83 2.7K//2.7K
Rpk1 R90 10K
Cff1 C89 220n//47n
Cff2 C81 470n//470n//220n
Css C90 470n
Ct C93 4.7n//470p
Cpk C77 150p
Ccp C99 100p//100p
Ccz C101 1n//150p
Cvf C79 470n//47n//10n

I am watching the mosfet's gate with a scope. When I enable the IC, I see a few pulses and then nothing.

When woking, I don't see a "6V DC and a little sine" at pin 6. I see 0,5-1V DC. I measured 7,5V (IC's reference) at pin 9.

I see a 1,8-2V DC at pin 8 and I think this is normal for 220V AC line.

I saw triangle wave at 52kHz at pin 14 so the oscillator is working.

I saw nothing at all at pin 5, but I think I should have seen something since this is the control system output.

When I remove the inductor (output voltage feedback is not coming) the pulses are coming but I think this proves nothing.

Is there something wrong with the values I used?

Can you point me a direction?

  • I think the issue is the diode D12 that you have in the voltage feedback circuit.
    Was there some reason that you added this part?
  • I saw D12, D14, D15 in a reference circuit but not using them. I am shorting the pads of D12, not soldering D14 and D15.

    Any other finding?

  • Hello,
    I am answering my own question. I am using UC3854B and the voltage feedback reference is changed with UC3854A&B versions. It's not 7.5V its 3V. So my Rvi and Rvd is wrong. I changed my Rvd to 4K7 and now its working.

    Now, should I use Rb1 or remove it?
    When I check the signals I see a lot of noise, (switching noise and high freq noise) what can I do to eliminate them or not being effected from them?
    Especially my peak limit pin 2 is noisy and it's reducing output voltage proportional to increasing power. I believe because of the noise, 3V is not 3V anymore it is 3,1V and with more current it is 3,2V so it is reducing more and more.

    Please try to understand and answer the questions.