For a 240VAC input and 5V/2A output to power an outdoor industrial application, is the UCC28710 the best solution if my highest priorities are reliability and ability to pass EMI testing? Size would be the next priority then efficiency and then cost? Is this a good selection for a new product with a 5 year warranty? Is there a way for Webench to recommend an off the shelf flyback transformer that's close to the one that Webench recommends? Thanks in advance! Dan T.