I am wondering can the UCC29002 be used to load share several power supplies that only output 12 volts and do not have external sense lines? I would like it to actively control mosfets to load share different power supplies. I require a single wire communication between the two different power supplies. Ideally I would like it function similar to the linear tech part LTC4370 but with a single wire bus like UCC29002 to go to n+1 modules.
Thanks for any assistance,