Hi
Our customer are evaluating UCC28070 as a bridgeless PFC. However the output voltage goes below setting voltage when the output power is increased over 1400W.
The condition is ; Vin=AC230V, Vo=385V, 1800W.
In the case of AC200V is no problem. However in the case of AC230 the output goes 340V when the output power is increased to over 1400W.
On the other hand, this phenomenon is improved if the Riom is increased to 27kohm from 19kohm.
We do not understand why. Could you give us any advises for this issue?
Regards,
Koji Hamamoto