Hi,
I am designing an output filter inductor for a 450V output full bridge converter. One of the required parameters for the area product when core saturated approach is used is the peak short circuit current. Is there any analytical method to determine it or any rule of thumb (percentage of the load current, ...). A reference to a technical paper on the subject would be very appreciated!
Also some specs of the designed converter (if one could help):
Vin = 400 V after PFC,
Vout = 450 V
Pout = 4.5 kW
dIL = 2 A (20% load current)
L = 750 uH
Thank you,
Florin!