We are investing AC input Oring DC240 to 360V is compatible with UCC28180 and UCC28051.
The DC input ripple is about 1V.
The Output voltage is 390V.
The output current is 1.6A for UCC28180 and 0.8A for UCC28051.
We would like to know recommeded DC input cuircuit for above condition.
Please advise if we can use the PFC compatible with DC input and any concern for this.
Best regards,
Hiroaki