the IOT trend asks for new solutions for power supply. While we try to decrease power consumption we will more and moer meet the limits of the power supply itself.
The efficiency of the available converters decreases dramatically if the output current decreases.
So if we limit the quiescent current to 4 mA the efficiency of the power supply will decrease to practically zero thus with a really bad overall efficiency.
Now the question: Are there new AC to DC or DC to DC converters that can offer high efficiencty at very low output currents?
this could be for instance 60VDC in and 3.3VDC out at 2mA
Or 230VAC in and 3.3VDC out at 2mA
that still have an efficiency higher than 60%
best regards
Robert