Hello Team,
I am working on a 30W AC/DC power supply requirement/ suggestion to customer, for which UCC28740 seems suitable device. I would like to understand how to configure following parameters on the design-
1. Minimum start up voltage of 80VAC : transformer primary inductance and turns ratio will determine this threshold or there is some additional component?
2. During power down power supply should switch till Bulk capacitor voltage on the input fall to 50V or 25ms of output hold up time:
Apart from choosing correct input and output capacitor, is there a way to configure this?
3. What parameters affect input to output delay or stat up time of the power supply? Customer requirement is 1.5Sec power up time, once the AC input is applied.
Regards,
Mahendra