Hi Everyone,
Here is my SPEC
Vin 135V , Vo 12V 45A Phase Shift full bridge
For test Over Voltage Protection, we found a problem.
When it work on no load, by adjust variable resistor output voltage will rise until trigger the external OVP circuit than turn off UCC28950.
But within load lower than 10%, after we adjust variable resistor, the PWM signal will shutdown automatically even the output voltage not rise to our target (14V), it shutdown at 12.6V
We went to know how it will turn off PWM automatically?
Thanks