Hello TI support team,
My question is in relation to the Design guide http://www.ti.com/lit/pdf/tiduas3.
On Page 9, under section 4.5
"The UCC28180 is a boost PFC IC by design; however, the flexibility offered by the IC makes it easily adaptable to control a buck PFC topology. This adaptation is possible by bypassing the current loop by placing a Zener-based constant voltage source at the ICOMP pin of the UCC28180 device. The user must be careful to ensure that the potential of the ICOMP pin is kept above 3 V"
1. Why does the current loop is bypassed ? Don't we need current loop compensation in Buck PFC or I am missing something?
2. And what happens when the current loop is bypassed and a zener of fixed value acts as a voltage source at ICOMP pin.
3. How does the sinusoidal shape of current is preserved in this case?
4. Irrespective of harmonic distortion or EMI complaince to IEC directives, can we use this buck topology using UCC28180 for power levels upto 1kw?
Thank you,
Abhishek