Hi,
I am simulating a simple 24V/12V converter in PSpice 16.6 using UCC28704. The simulation works very well for 1ms, then the UCC shuts itself down.
The VDD is always 24V. VS current draw, CS voltage range and VS voltage range are all within limit as shown in the following figure.
(Green: VS pin current. Blue: VS pin voltage. Red: CS pin current)
One strange thing I noticed is that the current draw of the VDD pin is zero during the simulation even when the chip is working for 1ms. I connected a 10M ohm resistor from the pin NTC/SU to ground.
Can you advise any reason of the device shutting down please? Thanks.
Zhenyu