I am trying to follow the application note at the end of the datasheet and then I will design an isolated flyback converter with my own parameters. I am using Mathcad 15 to make the calculations. These are some parts I couldn't understand:
1. After calculating Lpcrit (page 26), do we use it on any place else?
2. Do Lm (page 24) and Lp (page 27) are the same thing (transformer primary side magnetizing inductance)? I calculated that as 1715uH. Should we take it as 1500uH in the following equations (page 24)?
3. 120mV ripple of 12V is %1 ripple isn't it (page 23)? Or is it %0.1 (page 25)? When I calculate Cout for %0.1, I found the result as 1865uF not 2015uF, why?
4. What is the value of Pin? If Pout=12V*4A=48W. Or is it 12V*4,33A=52W. (4,33A is out current max, page 23). Now Pin=48/0.85=56.47W or Pin=52/0.85=61.13W? This affects the mosfet rms current...
5. In equation 30, what is the 100kHz expression? Is it our switching frequency which should be 110kHz? This affects the Rcsf calculation...
6. I calculate Go (DC open loop gain) as 5.59db, datasheet calculates 14.95db. We will use it on Ho(s) later. My bode plots are not the same with the ones in the datasheet. Maybe it is related with the Go calculation difference maybe not. Can someone explain this part?
7. I see in the schematic Rb1 and Rfb2 (page 22) but in page 29 there is a Rfb mention. Is it Rfb2? If so how do we calculate Rfb1 which is 4.99k in the schematic?
8. Can someone show me how to calculate Rled from compensation loop transfer function as explained in text (loop gain must be 1 at crossover freq.)?
9. For final bode plots (page 30) do I multiply G(s) with Ho(s)?