Hello,
I got following questions from customer.
Coulc you please put answers for those?
===============================================================================================
Q1) In page 1, there is a following description, but not mentioned in Electrical Characteristics parts in the datasheet.
“ Integrated Gate Driver With 0.4-A Source and 0.8- A Sink Capability”
Is this guaranteed specification?
Q2) In Table 1, DT port explanation, it says
“To prevent shoot through when this pin is accidentally shorted to ground, the minimum dead time is set to 120 ns. Any dead time setting less than 120 ns will automatically have 120-ns dead time.”
Is this 120-ns guaranteed value?
Can you show min/max value for this period?
Q3)Regarding to SS capacitor, 1uF is defined as recommended maximum capacitor.
In customer's application, longer soft start period will be required and more capacitor is required than 1uF.
- Is 1uF actual maximum capacitor for correct operation?
- Why maximum capacitor is defined as 1uF?
Q4) Regarding to “FSW(start)”, is this fixed value and user can not configure this value?
Q5) Regarding to “GATE DRIVE” specification, GD1, GD2 output voltage high is specified as 9V(min) to 11V(max).
Is this defined under the condition of VCC being between 11V and 18V?
Q6) “Thermal shutdown threshold” is defined as 160deg(typ), but absolute maximum ratings for Tj is described as 125deg.
Why thermal shutdown is defined as 160deg which is far above Tj max?
Q7) Customer wants to set switching frequency as 290kHz.
According to equation (18), required IRT will be
IRT = 290[kHz]/83[Hz] = 3.493mA
To get IRT of 3.493mA, RT resistance would be,
RT resistance = 2.5V/3.493mA = 0.715kohm.
- Is it correct understand?
In this case 0.715kohm is smaller than 1kohm, which is smaller than recommended RT resistance.
- What is the concern when using RT resistance under 1kohm?
Q8) What is OC_latch? Could you provide explanation for this?
Would OC_latch be connected to FAULT block in Block Diagram?
Q9) In section 7.3.1, it says "During soft start, the switching frequency is increased."
With followings, this expression makes the customer bit confusing.
- From Figure 12, switching frequency looks like decreasing during soft start.
- And Start frequency is fixed at 142.5kHz with regardless with RT resistance.
Is this based on the assumption that operating switching frequency is typically higher than 142.5kHz?
========================================================================================
Best Regards,
Nobuo Fujihara