Hi team,
OUTC and OUTD pulse width issue are occasionally occurred in the UCC28950 application.
The measured waveform is attached.
This application is designed as an 1100W power.
The issue occurs from about 100W to larger load conditions.
I am considering that in this case, load condition is a little light compared to the Dmax issue of UCC28950.
What kinds of problems are considered?