Hello all,
I have designed an AC/DC power supply using the part number UCC28711D. The voltage input is 220Vac and the output is 5Vdc.
The schematic used is the same of the reference design (you will find attached).
The startup of the system is very slow, it takes around 7 seconds to get the 5Vdc at the output. In addition, as soon as I connect the load, the voltage at the output drops at 3,3V and slowly grows up to 4,1V until drops down to 3,8V, repeating the cycle again and again.AC-DC schematic.pdf
Please, could you help me with this issue?
Thank you so much,
Joaquín