Dear,
Firstly, please help take a look at the attachment for our AC-DC design, this design is base on one of TI UCC28740D reference design, convert 85V-265VAC to 5VDC@3A.
The design is working well so far, the next step is that we want to reduce the BOM cost and want to change some components on our design. In AC-DC design, we was using a Wurth Common Choke as a EMI filter at VAC input, this choke's price is little high and we want to replace with the cheaper one. The RefDes of the Choke is L44 in our schematic.
1/ Wurth Common Choke (PN: 7448012501) Spec's:
a. 1mH @ 10kHz
b. Current Rating: 2.5A
c. 55mOhm
d. VAC rating: 250V
2/ The new one - Kelmet Common Choke (PN: SC-01-10G) Spec's:
a. 1mH @ 100kHz
b. Current Rating: 1A
c. 70mOhm
d. VAC rating: 250V
Question: Is the Kelmet Common Choke good enough to replace the Wurth's one? Do you think current rating 1A is enough for this circuit?
Attached datasheet of both Chokes for the reference.
Please help give me any ideas.
Thanks and Best Regards,
Hoang