Recommend HS voltage range is specified from -8V (MIN) to 600V (MAX) at HB-HS=12V in datasheet page 5.
Customer inquired that there are recommend HS voltage specifications for a negative pulse with such as 1us, 500ns, 100ns, 50ns etc. width?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Recommend HS voltage range is specified from -8V (MIN) to 600V (MAX) at HB-HS=12V in datasheet page 5.
Customer inquired that there are recommend HS voltage specifications for a negative pulse with such as 1us, 500ns, 100ns, 50ns etc. width?
Thank you for prompt response, I got the Figure 53.
I have some more questions.
(1) What does plus/minus voltage of the vertical scale mean?
For example, does ±20 corespond to -20V negative pulse?
(2) Figure 53 specification is for HB-HS=15V.
What does specification become for HB-HS=10V (MIN) to 18V (MAX)?
(3) Recommended HS specification is -8V(MIN) to 600V(MAX) at HB-HS=12V..
What are recommended HS specification for HB-HS=10V(MIN) to 18V(MAX)?
(4) Negative voltage feature makes a plateau for wider pulse width than 500ns in Figure 52.
What does this plateau mean?
How does this plateau value differ from DC HS minimum specification of -8V on page 5?