Other Parts Discussed in Thread: , UCC3817, UCC3817A
Dear All:
I use UC3854 for PFC bus,when I test the U0,the value are different between different device .The schematic as follows:
The sample 1 voltage waveform as follow:
1、Device start
we can see the voltage on bus U0 is 378.5V-361.5V,∆U is 17V, the cycle is 3.4s.
2、Sample 2 voltage wave( I just change another UC3854).
we can see the voltage on bus U0 is 386.5V-378.5V,∆U is 8V, the cycle is 1.5s.
I want to kown why the test value are different between different chips?Is there something wrong in my design?Do you have Any good suggestions for improvement.Thanks a lot!