Other Parts Discussed in Thread: UC3842, UCC2803
Question regarding application of UCC2800 series:
1) Can I use it in a boost application? I do not see any conflict , given that its max D is almost 100% & control is the same scheme as in x84x family i.e. UC3842 or 43 etc
2) If I can then, why can it not be used to drive GaN power devices? I can add external components t source & sink. There s no need to go negative at gate, a fast schottky will suffice, wont it?
3) If these cannot be done with UCC2800, can you suggest a device that can? I need operatin down to 5V...maybe 6 to be directly compatible with GaN gate drive.
robin