Other Parts Discussed in Thread: TINA-TI
Hello everyone,
I am trying to design an AC/DC isolated PSU. I want to use an off-the-shelf transformer, I found 750811613 from Wurth that might meet my requirements.
My requirements are to have a universal AC input and 2 outputs 1.6A@5V and 0.6A@12V.
I have few questions :
1- If I use the UCC28704 calculation sheet provided by TI (sluc603b) and make the calculations for one output the 12V for example. For the current consumption I will use the sum of both. In the fields for the secondary winding I will use the ones for the 12V winding, in the primary and auxiliary fields I will use the one provided by the wurth datasheet exactly. The 5V winding should follow the 12V winding on its own ? Will this calculations work ?
2- Is it possible to simulate the above circuit ? Wurth provides an encrypted LTSpice model while TI provides an encrypted PSpice model. Can these two models be made to play together ?
If not can I simulate the Wurth transformer in TINA-TI or Workbench or any other tool ?
3- In general is this transformer suitable for this application ? I read few application notes that "The secondary voltage should be higher than the target voltage, otherwise the target output voltage will be unrealizable. ". When Wurth datasheet states 12v does it mean I can have a target voltage of 12V or my target voltage should be less ?
4- I found other calculators/tools/application notes that require the transformer core and the number of turns. Wurth does not provide this information. TI sheet does not require these entries, only the ratio of turns and inductance. Does this impose any limitations on TI sheet ?
Thanks for any help, sorry if my questions sound idiotic :D .
References:
1- Wurth transformer datasheet
2- TI UCC28704 Calculation sheet: