Other Parts Discussed in Thread: PMP
HI,
I asked about the startup circuit with the following thread.
e2e.ti.com/.../590291
The starting circuit refers to PMP 5141, but PFC is unnecessary.
I think about deleting as shown in the attached diagram, but are there any problems?
I am considering the following AC / DC circuit in another project.
I would like to refer to PMP 5141 for this matter as well. However, since the area of the board is narrow, I do not want to use the PFC circuit.
Is it OK to not use PFC with the following specifications? What is the problem when not using PFC?
Specification (AC / DC converter)
Input / output condition ① (initial setup)
Input: AC 80V ~ 120V
Output: DC 24V 6A
Input / output condition ② (Voltage rises to ② after a certain period from startup)
Input: AC 180V ~ 240V
Output: DC 24 V 12.5 A
Best regards,