This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2895: Resonant ringing seems excessive. Is this normal?

Part Number: UCC2895

I am developing a 3000 Watt dc/dc converter, 48 Volt nominal input, 200 Volt output.  A planar transfromer has been implemented with a four-turn primary and a 22-turn secondary (although the secondary turns need to go up on re-spin).  There is no shim inductor (although I can add one).  the leakage inductance is about 500nH, the resonant frequency is about 925KHz.  

I am noting excessive ringing on the primary waveforms at the resonant frequency, as shown in the scope plot below (hopefully it uploaded correctly).

The plot shows operation with a 50 Volt input and an 870 Watt load.  Channel 1 is the A Upper gate drive signal from the 2895; Ch2 is the primary current as measured by a current transformer. Ch3 is also the primary current, as measured by a TCP2020 current probe.  Ch4 is the primary voltage (bridge output).  

Note the ringing at what I believe is the resonant frequency.  Channel 4 shows a peak of 73 Volts, and Channel 3 shows a 34.4 Amp peak-to-peak ripple.  

From what I understand there should be some resonant component to the voltage and current waveforms, but this seems excessive.  Are these waveforms typical for this converter toplogy?  If not any idea what I can do to resolve this issue?  I believe the ringing and current magnitude are causing excessive power dissipation in my primary and secondary windings, as they are getting quite hot.  

Thanks in advance for any assistance.  

tek00251.tif

tek00245.tif