hi
have some question about UCC28910,thanks a lot for helping me.
describe :
1、 i use UCC28910 input 220v AC, and output is 4.2v, the shcematic as below
2、the load of output is for MCU module,usual the current is 30mA,but when the RF-ZigBee module work, the current up to 100mA
3、when the current 30ma up to 100ma the ouput voltage has a short drop, from 4.2v to 3v. and the test as below, the red is output voltage, the blue is Vs
question:
1、What caused the voltage drop ?
2、I guess that UCC28910 work on DCM (when current is 30ma) ,and normal mode(when 100ma).
so how long does DCM change to normal mode ? what will affect the time ?
and what is the transfer function model?
thanks very much
and best regards