This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD3138HSFBEVM-029: UCD3138HSFBEVM-029:

Part Number: UCD3138HSFBEVM-029
Other Parts Discussed in Thread: UCD3138

Hello,The《Using the UCD3138HSFBEVM-029 User's Guide》"A.5.2 Prebias Load and Load Synchronous Startup",tell us"The special technique, called Synchronous Startup, is used to enhance the parallelstartup performance of UCD3138 controlled converters. This technique uses a GPIO pin as sync-pin which connects each board together to start at the same time then the output voltage difference from different converter is minimized."

I have a question about the function of synchronous startup。How to design the hardware and the software to achieve synchronous start function?thanks。