Other Parts Discussed in Thread: TL431
Using UCC2897A design a DC/DC power supply, but now the power supply can't load(just can load about 50mA )
the arguments of the DC/DC are as below:
INPUT: 60-100VDC
OUTPUT: 48V/10.5A
Debugging
1, DNP the TL431 CC loop
2, cancel the CT, using the resistance to detect the current in low-side MOS
Question:
1, Any Suggestions for debugging?
2, Any suggestions for Transformer designning? could you provide the calculation for UCC2897A transformer design?
the sch and the transformer drawing are attached.UCC2897A sch and transformer.docx