Hi all,
I am trying to select a DC/DC non-isolated converter that will work with 12V or 24V DC input voltage
The Vout should be 19V DC and the output current 0.5A
I guess that a buck/boost converter could maintain the output voltage in both cases, 12V or 24V of input voltage. My concern is when the input voltage is 12V because it is 7V below the required 19V of output
Is a buck/boost converter a suitable component for this application?
Thank You!